Hi All
I used pairing / bonding in a multirole app running on CC2642.
If I connect to a central (Mac OS for instance), pairing and bonding works as expected.
When I reconnect, no issue.
If I erase bonds (mass erase flash for instance) on the peripheral side only, reconnection to the same central fails, and I receive a GAP_LINK_TERMINATED_EVENT with error 13, immediately after the GAP_LINK_ESTABLISHED_EVENT.
If if forget the device on the central side, I can reconnect through pairing / bonding.
I'm using SDK 6.41.0.17
How can this be solved ?
Thanks