Part Number: CC1352P7
Other Parts Discussed in Thread: SIMPLELINK-CC13X2-26X2-SDK
Hi,
I have two LP-CC1352P7 development kits for thread function evaluation.
The thread function works properly when I use the thread example "door lock" in the SIMPLELINK-CC13X2-26X2-SDK .
Now I want to add BLE function in the "door look" example. We want to use BLE app to set up development kits as the roles of gateway and device.
Where should I start from the examples?
Will there be any Flash size issues if BLE and Thread are integrated into the image?
Rick