Part Number: LP-CC2651R3SIPA
If AT command is sent, then which format of command will send over module by UART?
only data part or with command also sending? frame format?
Board:
UBLOX ANNA/NINA-B41x
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LP-CC2651R3SIPA
If AT command is sent, then which format of command will send over module by UART?
only data part or with command also sending? frame format?
Board:
UBLOX ANNA/NINA-B41x
Hi,
AT commands should have both the command and data part.
Which AT firmware are you using?
Is it with our example, rfDiagnostics?
If yes, please see the example README for more details:
https://dev.ti.com/tirex/explore/node?node=A__ACJsd29-81ykPxmgaN.V3A__com.ti.SIMPLELINK_CC13XX_CC26XX_SDK_PROPRF_MODULE__BSEc4rl__LATEST
Thanks,
Toby