This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652RSIP: CC2652RSIP 1.8 V power

Part Number: CC2652RSIP
Other Parts Discussed in Thread: CC2652RB

Hi Team,

I wanted to confirm if CC2652RSIP and CC2651RSIPA can run of 1.8 V power supply. Currently using CC2652RB, which has a spec for an external regulator mode to operate in 1.8V input as shown below from the datasheet.

Neither CC2652RSIP nor CC2651RSIPA have that same specification shown below, but my understanding is that these devices are similar/ the same core.

Can both of those be powered with 1.8 V supply?

Thanks!