Other Parts Discussed in Thread: CC2640, CC2650, LMP91000
Hi...
In a related discussion I was asking about porting an older project based on the 8051 to the cc2640/cc2650.
So where we went with that is to go new development totally and so we ordered a LMP91000 eval board so we could plug our 3-prong sensor into it..
I was able to get the I2C project working on the CC2640 and was able to program the LMP91000 and actually measure gas changes on the sensor..
However I am trying to integrate the I2C project which is TIRTOS based woth the BLE PROJECT ZERO..
and I have issues.. I stay away from calls to the GPIOs GPIO_init() as that totally causes the PROJECT ZERO to lock up.
I added I2C_init()
However while this kinda works then other things dont work.. like I think the BLE stilll gets messed up..
How do I integrate I2C into the BLE projects (like project zero)
and I will also need to add to read from the ADC also...
(everything can be polled for now)
I2C project is I2Ctmp_CC2640R2_LAUNCHXL_trtos_ccs.. (I basically only changed the I2C messages to the temp sensor to be the ones I need for the LMP91000.. that work great...
the BLE is the stock project ZERO.
John