Part Number: CC2340R5
SDK version: 7_10_00_35
I have two questions:
1.
Is the Flash Erase range of CC2340's ROM Bootloader unable to be changed?
During the test, I found that the ROM Bootloader uses the Command method to make the CC2340 Erase
Does this mean that every time Erase can only Erase all, and cannot select a range?
2.How to use Code to determine whether GPIO is currently in a HIGH or LOW state?