Other Parts Discussed in Thread: BLE-STACK
Hi, TI_Team.
Please let me know the timing of events that occur during advertising packet transmission.
I have confirmed the operation of the software with the additions of "BLEAPPUTIL_ADV_END" and "BLEAPPUTIL_ADV_TERMINATED" to the event handler.
I am toggling a port at the timing of event occurrence.
As shown in the diagram below, it can be seen that "BLEAPPUTIL_ADV_END" event occurs both before and after transmission,
while the "BLEAPPUTIL_ADV_TERMINATED" event occurs after transmission.
@SDK 7.40

Q1.Why does "BLEAPPUTIL_ADV_END" occur before transmission?
-Does the fact that the API: GapAdv_disable() is executed before transmission have any effect?
Q2.Why does "BLEAPPUTIL_ADV_TERMINATED" occur?
I have made the following settings, but I would like to know if the cause "Sent when an advertisement set is terminated due to a connection establishment" will trigger
the occurrence of the "BLEAPPUTIL_ADV_TERMINATED" event?"
-Device Role:Broadcastaer、Legacy Event Properties Options:Non-connectable and Non-scannable undirected
Please feel free to ask your question, and I'll be happy to provide a response.
Regards.