Hello,
For CC2640R2F or CC26xx family uC, there are two modes of power operation, namley "normal operation" mode (3.3V), where an internal LDO is also used as VDDR, and external regulator mode, where external 1.8V regulator is used for all supplies, VDDS/VDD2-3/VDDR. Do you guys know of any data or table in regard to advantages in power consumption for either mode? I understand that actual consumption may depends on multiple factors. But a ballpark comparison would be a quite informative.
Many thanks!
Albert