Part Number: CC2652PSIP
I am currently using the example of simple_mesh node and want to understand the actions running in it by opening BT_DEBG of zephyr.
Is there a quick way to enable it, or what settings do I need to make to enable it?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CC2652PSIP
I am currently using the example of simple_mesh node and want to understand the actions running in it by opening BT_DEBG of zephyr.
Is there a quick way to enable it, or what settings do I need to make to enable it?
Hi, BT_DBG is already enabled however you need to provide your own logging function in "Mesh/zephyr/include/logging/log.h"
I suggest you take a look at this FAQ: [FAQ] CC2642R: Tips and tricks to use "BLE_LOG_INT_" functionalities - Bluetooth forum - Bluetooth®︎ - TI E2E support forums to enable logging features.
I hope this help
Tanguy
Hi Tanguy,
Thank you for your reply.
So, if I understand correctly, I need to study the methods and functionality provided in osal.c and then adapt or replicate them to implement the desired functionality in log.h, is that correct?
Regards,
Neil
Hi Neil,
You don't have to replicate them you can just call them. But you may have to use wrappers around because I am not sure the 2 Api are directly compatible.
Regards,
Tanguy