Hi
SDK Used : simplelink_cc13xx_cc26xx_sdk_7_10_01_24
Code Used : simple_peripheral_LP_CC2652R7_tirtos7_ticlang
Chipset Using : CC2652R7
In the simple peripheral code 0xFFF1, 0xFFF2, 0xFFF3, 0xFFF4 and 0xFFF5 UUID's are used for Read, write and notify purpose. Shall i continue with the same UUID for Huge Mass production or Any UUID to be purchase ? or Any Unique 128-bit UUID to be used ?
0000FFF1-0000-1000-8000-00805F9B34FB - In general this UUID is mentioned as "Bluetooth SIG-defined GATT profiles". Will be face any problem on this ?