Other Parts Discussed in Thread: CC2640
Hi Team,
We have used CC2642R1FRGZ device in one of the project and interface that device to another host via UART communication & some handshake signals via port pins.
Basic interface is working we are able to communicate CC2642 to another host via UART.
Running this HW Qualification tests high /low temperature (-40 to +85).
Found some observation during high temp testing (Duration is 24 hours). when HW is power cycled (Turn ON/OFF power to HW) during high temperature operation drawing high current & unable to communicate via UART. Some HW devices we are able to comminate when HW is back to room temp and some HW devices showing fail.
Please check once below sch & suggest any improvements needed.
Regards,
Rajani