This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all
I'd like to use the FET3410 to flash the boards from the eZ430-CC2560 kit as I cannot get the virtual serial port to show up on the Mac. The FET430UIF works more or less, and is supposed to support spy-by-wire and on the battery holder of the kit, there are nice 2.54 mm pads to solder a connector. Now, what connections do I need to make? The datasheet on the MSP-FET430UIF doesn't even have a pin-out of the JTAG cable.
Could you post a quick explanation with labeled pictures?
Best
Matthias
Matthias,
Could you clarify your question. What hardware do you want to use to program the EZ430-RF2560?
BTW, there is access to JTAG using the uEVM connector on the back, as you can find in the wiki:
http://processors.wiki.ti.com/index.php/EZ430-RF2560
Regards,
Gustavo
Hi.
Ok, I try again.
I want to program the "Target Board" of the eZ430-rf2560 kit (http://www.ti.com/tool/ez430-rf2560) using the msp-fet430uif (http://www.ti.com/tool/msp-fet430uif) over the Spy-by-Wire pins available at the battery holder of the eZ430-rf2560 kit as I cannot get the provided eZ430-FET to work on the Mac.
I've seen the uEVM connector, but I have nothing to solder there and I'm also not confident that I would be able to solder that. The Spy-by-wire pins on the battery holder are normal 2.54 mm through-hole pads - I can solder those.
Basically, I (and everyone else) is missing the pin out of the JTAG port on the msp-fet430uif. The datasheet shows how to connect the target but doesn't give the JTAG pinout.
Thanks
Matthias
Matthias,
You can see an example of pinout on any experimenter board:
Take a look at here:
http://www.ti.com/litv/zip/slac228
Open the files in Eagle: www.cadsoft.de and you can see the orientation in which the cable will fit and which pins are what.
Regards,
Gustavo
Gustavo
good idea.
So, the schematic is
And the snippet from the board is
So, PIN 1 is the rightmost in the upper row, when looking at the JTAG connector from the frontside and I'll need Pins: 1 TDO/TDI, 8 TEST/VPP and 9 GND. Plus Pin 4 VCC Target, if I want to power the target too.
Add on question: do I need the R1 47k Ohm resistor between VCC (pin 4) and TDO/TDI (pin 1)? It looks like it would be part of a normal Reset circuit?
Just wanted to confirm that the proposed solution actually works using the schematic that was pointed out earlier. I used JTAG pin 2 to power the target board and left out the fuse blowing stuff, as explained in the notes.
I've also connected the Debug UART to an FTDI USB-2-UART which isn't limited to 9600 as the original eZ430 FET.