Part Number: CC2340R5
CCS version : 12.7.0
SDK version : 7.40.00.64
As a peripheral, I set 1000ms as the advertising interval in Syscfg. However, when CC2340 is scanned and enters the event BLEAPPUTIL_SCAN_REQ_RECEIVED and advertise ScanResData, I find that the advertising interval will become 20ms. Is there any way to change this 20ms? Or Is this a fixed value of Scan Response?