Part Number: CC2564CSTBTBLESW
Other Parts Discussed in Thread: CC2564C
Hello,
I have a problem with HFPDemo_AG application running on our STM32F4 custom board with CC2564C. Bluetopiastack CC2564CSTBTBLESW-v5.1.1.1
Application not works with Samsung SM-R180 EarBuds2. With several other commercial headsets, the app works fine.
After opening the HandsFree port, the connection is terminated.
Here is log from terminal:
HFP AG>openaudiogatewayclient 1 6
Bluetooth Device Address: 0x64037F1A9401
Open Remote HandsFree Port = 0006
HFRE_Open_Remote_HandsFree_Port: Function Successful ID = 0004.
OpenRemoteHandsFreePort: HFRE_Update_Current_Control_Indicator_Status Function Status 0.
HFP AG>
atLinkKeyRequest: 0x64037F1A9401
GAP_Authentication_Response() Success.
HFP AG>
atAuthenticationStatus: 0 Board: 0x64037F1A9401
HFP AG>
Unknown/Unhandled GAP Event: 1.
HFP AG>
HFRE Open Port Confirmation, ID: 0x0004, Status: 0x0000.
HFP AG>
HFRE Close Port Indication, ID: 0x0004, Status: 0x0001.
I am also attaching the log from TX Debug pin captured by TI Logger.
Interesting think is line #1096 LMP_Detach and several lines above.
Best regards
Pavel Novotny