This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-EM-CC1354P10: ProjectZero on board not starting

Part Number: LP-EM-CC1354P10
Other Parts Discussed in Thread: CODECOMPOSER, CC1354P10

Just received the launch-pad and the XDS110ET. I have just connected them as described in the user-guide. Jumpers have been set as requested and verified in the schematics (default). I was expecting, that the "out-of-the-box example" (ZeroProject) will start, but I didn't see the device on the SImpleLink-App and there was nothing in the console window (putty). Using the User-guide, I tried to restore the "out of box experience", following the instructions to install the browser plug-in and TICloudAgent. The progress bar runs until 20%, then disappears. No success or error message - and still no reaction on the App after resetting the board.

The I installed the SimpleLink CC13xx-cc26xx-SDK (7.40.00.77) and imported the ProjectZero-example on CodeComposer 12.7.1, compiled it and uploaded it on the board. Using the debugger, I can see, that in icall.c the function ICall_waitMatch() returns ICALL_ERRNO_TIMEOUT and thus calls ICall abort() which is an endless-loop.

Now I am stuck - did I receive a defect board or did I forget something to set-up the board?

Regards

Klaus