Tool/software:
Hi Team,
My customer is using CC2340 and they want to modify the TX power to +8dB during connections at DTM mode.
Please help to to check:
1. if TX power need to set as +8dB, the command parameters of HCI_EXT_SetTxPowerCmd is 17?
2. Can the commend: HCI_EXT_SetTxPowerCmd() can be launched during BLE connection, not just before connection ?
Thanks.