Tool/software:
Hi,
I am working CC2650 PFB the other details,
CCS Version - 7.4
Stack Compiler Version - 16.9.6.LTS
Bim Compiler Version - 16.9.6.LTS
Application Compiler Version - 5.2.6
BLE SDK Version - ble_sdk-2_02_07_06
i am facing the problem in OAD update,
for example - if i flash the firmware from my PC's CCS and later if i want to update the firmware using .bin file over OAD (*Note - .bin file is generate from another PC's CCS) then OAD update is not completed successfully, if i do the same with .bin file generated in my PC's CCS then OAD update is completed successfully.
so, i need help in how to generate merge bin file of BIM+Application+Stack,
kindly, guide me what is step to generate merge .bin file and what should be post build steps, where to add and how to add.
Regards,
Rajnish Singh