Part Number: CC2642R
Tool/software:
Hello, I am implementing multiple peripherals in the mutlrole example.
1. When implemented using Launchpad, advertising is observed and connection is possible even when multiple devices are connected. If you apply the same example program to a board designed with CC2642, there is a problem that advertising cannot be observed when one device is connected.
2. The connection speed is so slow that you have to wait for more than 1 minute. There are times when connection is not possible even after more than 1 minute.
Is there a way to fix the above problem?