I found out, the USB dongle with the HostTestRelease-software scans somehow all the advertising channels. But what I don't understand how does this works... I think the scanner makes a TDMA on the three channels. Or is he scanning on the three channels all the time?
So I would like to make 3 scanners. Each working on ONE of the advertising channels.
1) Is this possible with the HostTestRelease workspace?
2) Is this ok for the BLE- standard?
4.4.3 Scanning State
The Link Layer shall enter the Scanning State when directed by the Host.
When scanning, the Link Layer shall listen on the advertising channel indices.
There are two types of scanning, determined by the Host: passive and active.
There are no strict timing or advertising channel index selection rules for scanning.
During scanning, the Link Layer listens on an advertising channel index for the
duration of the scan window, scanWindow. The scan interval, scanInterval, is
defined as the interval between the start of two consecutive scan windows.
The Link Layer should listen for the complete scanWindow every scanInterval
as directed by the Host unless there is a scheduling conflict. In each scan window,
the Link Layer should scan on a different advertising channel index. The
Link Layer shall use all the advertising channel indices.