This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2340R5: How to implement long-range using coded PHY BLE feature.

Part Number: CC2340R5

Tool/software:

Hi,

For the new generation Bluetooth Smart chipsets (and modules) based on CC23xx supporting Bluetooth 5.3 LE Long range (coded phy 125kbps) feature, I would like to understand a bit more and wonder if you can help me out here.

I want to know more about it, normally we use 1Mbps for CC2642R1 in simple Peripheral mode (Legacy and Extended advertisement in 5dbm Tx power)

But now we are currently working on the CC2340R5 device in that we need coded Phy for long range feature so for that we have to change in both central device and peripheral device.

so, need to know what changes required in system configuration for both central and peripheral device.

Code composer studio v12.5.

SDK version: simplelink_lowpower_f3_sdk_7_40_00_64

please helps us for the same.

Thanks, and Regards

Balaji Wankhede