This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2340R5: ADC interrupts and DMA

Part Number: CC2340R5
Other Parts Discussed in Thread: SYSCONFIG

Tool/software:

I can see from the reference manual that the ADC can independently scan through channels, generating interrupts to let the cpu get the data or even use DMA. I cannot see this functionality anywhere in the SDK. Am I missing it or are these features not supported in the SDK?

Are there any examples at all using the ADC interrupts and/or with DMA with or without the SDK?

(For clarity, I do not mean triggering the ADC conversion from a timer interrupt)