Part Number: CC2540
Tool/software:
BLE-CC254x-1.5.2.0
Update 6/19/2024 - When I comment out these lines, the error went away. Question - Why would these codes cause linking error?
//-Z(CODE)ALIGNED_CODE|2=_CODE_BEG-_CODE_END,_BANK1_BEG-_BANK1_END,_BANK2_BEG-_BANK2_END,\
//_BANK3_BEG-_BANK3_END,_BANK4_BEG-_BANK4_END,_BANK5_BEG-_BANK5_END,_BANK6_BEG-_BANK6_END,\
//_BANK7_BEG-_BANK7_END
6/18/2024
I am seeing following error during linking when I use this linker configuration file: cc254x_f256_sbl.xcl.
Linking
Tool Internal Error:
Internal Error: In function: unknown
Diagnostic: unexpected exception
P0:1 P1:0
Error when running linker.
I don't see this error when I compile using IAR10.30.
I also don't see error when linking my project with other XCL file, for example ti_51ew_cc2540b.xcl.
Any idea how to fix this? Thanks.