Hi
I would like to create an application with a lot of BLE-devices and a few BLE-scanners. My BLE-devices are all in the advertising-mode. They send there data in the payload of the advertising-packet.
1)Is ist possible to set some parameters on the workspace "Host Test Release---CC2540USB Master" to scan just on one of the three advertising channels? I know this is not exactly BLE-standard... But when I build 3 scanners, each listening on one advertising-channel I will get more advertising-packets. I think this is somehow possible, beause the sniffer is also possible to scan just one channel... Is there a possibility to connect with a Java-application to the USB-Dongle in the snifing mode?
2) What is a scanWindow exactly? I think it is the time on which the scanner is listening on one of the three advertising-channels. Is that right?
At the moment I'm working with the Btool. But I also wrote a Java-application which got the possibility of scanning.