Other Parts Discussed in Thread: CC2540
Hey Team,
My customer is using the BTool sofware to communicate with the CC2540 Bluetooth LE module and is getting the following error:
GAP Device Initialization Timeout.
Device May Not Function Properly.
The issue seems to be with either the chip or the pathway between the chip and the RS232 Serial port. they are unable to initialize and communicate as a GAP device. I've done extensive testing with a number of different serial configurations but all have ended with the same result. If you are aware of any issues involving this combination of development tools or the BTool software, it would be much appreciated.
The RS232 connection is functional because the customer's UART code seems to have no trouble sending or receiving. It's just the HostTestRelease program that is not communicating back to the serial port.