I've asked this question over in the C5000 forum but haven't gotten a response yet.
Is there are Bluetooth solution for the C5000 processors? This post http://e2e.ti.com/support/dsp/tms320c5000_power-efficient_dsps/f/110/p/122469/436507.aspx#436507 indicates that there is but doesn't provide any details. This post http://e2e.ti.com/support/dsp/tms320c5000_power-efficient_dsps/f/109/p/133626/483889.aspx#483889 also mentions that the PAN1315 Bluetooth module is compatible with the expansion header on the C5535 eZdsp development kit.
The missing piece of information is the details on the Bluetooth stack that can be used with this platform. Is it the same Stonestreet One Bluetopia stack that is used on the Stellaris platform? I assume that it would need to be compiled specifically for the C5000 processors and couldn't be copied from the StellarisWare distribution. Any pointers in the right direction would be appreciated.
Cheers
Adam