Part Number: LAUNCHXL-CC2640R2
Tool/software:
Hi I found this old thread (see related question) that says that executing BTool through mono is not supported anymore.
Maybe it would be a good idea to remove the readme.txt that suggests this is possible from the SDK? Because I certainly went on a wild goose chase trying to make this work...
Also count me as a +1 for having more tools that are not 100% reliant on windows to operate!
Munan
=========================================== Texas Instruments BTool =========================================== ------------------------------------------- BTool - (For Version 01.42.00 or higher) ------------------------------------------- ------------------------------------------- Integrated Cross Platform Runtime Executable (Using Mono 4.8.1) ------------------------------------------- 1. Install BTool in Windows. (Note: Mono is NOT needed in Windows) 2. Copy the installed files btool.exe btool.exe.config btool_gatt_uuid.xml btool_config.xml as is, to a different OS with Mono installed. 3. Run "btool.exe" using Mono on the different OS. Tested using Windows XP, Windows 7, Ubuntu 12.04 LTS, Ubuntu 11.10. Should be usable under Linux, Mac OS X, BSD, Sun Solaris, Android, PS3, Xbox 360 and more! See http://mono-project.com/What_is_Mono for more information. =========================================== Getting BTool Running In A OS Other Than Windows =========================================== Install Mono 4.8.1 Follow instructions here to get latest mono via apt-get http://www.mono-project.com/docs/getting-started/install/linux/#debian-ubuntu-and-derivatives sudo apt-get install mono-complete sudo chown <user_name> /dev/ttyACM0 or sudo chown <user_name> /dev/ttyACM1 Using a terminal window, change to the directory where the files are and issue the following command: mono btool.exe