Tool/software:
Hi ,TI:
Currently, our company is using CC2340 and CC2745 for project development. In accordance with the requirements from the client, we need to sign a FOSS declaration document. We have scanned the SDK provided by TI using BLACKDUCK and found the following open-source code. We hope TI can assist in providing a solution.
We have scanned a total of three SDKs and detected the same open source code issues in all of them. Here is a list of inferred reasons based on the scan results.
No. | Components | Source | Match Type | Match Score | Usage | License | License Risk | Security Risks | Operational Risk | BlackDuck Recommendation and FII's requirements |
1 | ble_examples simplelink_cc2640r2_sdk-4.10.00.00 | 1 match | The file has been modified. | 4% | Dynamic Link | LGPL-2.1-or-later | Medium | High | FII:Scan results indicate a high-risk associated file in the SDK's \SOURCE\TI\ble5stack_flash\common\cc26xx\time directory, but no associated files were found in that directory. However, the code in this directory is identical to the code in the time directory of the ble_examples simplelink_cc2640r2_sdk-4.10.00.00 project on git. Both sets of code in the TIME directories have licenses provided by TI, without LGPL licenses. Did TI adopt the LGPL license to provide this segment of open-source code? If so, can FII declare only the TI license? Or can TI provide alternative solutions without LGPL? | |
2 | FreeRTOS Real Time Kernel V10.5.1 | 16 matches | Accurate Index | 79% | Dynamic Link | MIT | High | Low | BlackDuck:This version has obvious vulnerabilities and needs to be updated to version V10.6.2 or above. FII:We hope that TI can update this code in the SDK to the new version or provide us with code that meets the update requirements. |
|
3 | mcuboot MCUBOOT_062_RC4 | 2 matches | The file has been modified. | 7% | Dynamic Link | Apache-2.0 | High | BlackDuck:This version was updated on April 16, 2020, and it is recommended to update to a newer version. FII:We hope that TI can update this code in the SDK to the new version or provide us with code that meets the update requirements. |
Note: We have scanned three versions of the SDK as listed below.
1.simplelinklowpower_f3_sdk_8_10_00_63_ea
2.simplelinklowpower_f3_sdk_8_10_00_46_eng
3.simplelinklowpower_f3_sdk_8_10_00_01_ea
have a good day!
james
2024.08.01