Tool/software:
Hi guys,
Due to some erroneous production step, some of our CC26X2R based boards feature an inaccurate crystal.
We measure them with the vanilla project zero code, where we add code to re-route the 32 kHz crystal to an output pin. We measure such output with a high-precision frequency counter.
For example, a bad value we see is 32772 Hz. The good value should obviously be 32768 Hz
I am not asking about how to solve this. Instead, I was wondering if someone could list the effects such oscillation offset can provoke.
For example, could this be the reason that a board with one of this "bad" oscillators takes more retries to connect (or it does not even connect) via Bluetooth?
Please, let us know.
Have a nice day.