This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2642R: How to direct the internal 48 MHz RCOSC_HF of CC2642 to a GPIO for output measurement

Part Number: CC2642R

Tool/software:

Hi Sir,

I use the SDK Version:simplelink_cc13x2_26x2_sdk_5_10_00_48.

BLE5 example : simple_peripheral


How to direct the internal 48 MHz RCOSC_HF of CC2642 to a gpio for output measurement?
For example, we have measured an external crystal 32KHz exported to a GPIO for output measurement, the example is as follows:
IOCPortConfigureSet(IOID_26, IOC_PORT_AON_CLK32K, IOC_STD_OUTPUT);
AONIOC32kHzOutputEnable();
Does RCOSC_HF have a similar API for calls?

Thank you.