Part Number: CC2340R5
Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
I've mass produced 180 boards so far, and found that there are 20 or so units with high standby current, the normal standby current is around 20uA, while the high ones are ranging from 30-100+uA.
What could be the problem?
The program works in peripheral mode, broadcast interval 1s, the program is modified based on basic_ble.
The board with high standby current will work fine if I change the chip for it.
I'm not sure if it's a chip problem or a program problem.
Doubt the program, most of them are normal.
Suspect the chip, TI's chip failure rate is so high?
Seek help from TI official technical support.