Part Number: CC2340R5
Tool/software:
Will the CC2340R5 RSSI value change as the communication rate changes? For example, if 200Kbps and 2Mbps are at the same distance, are the RSSI values the same?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CC2340R5
Tool/software:
Will the CC2340R5 RSSI value change as the communication rate changes? For example, if 200Kbps and 2Mbps are at the same distance, are the RSSI values the same?
Hi,
Assuming the same transmit power and modulation schemes are used, the communication rate should not impact the RSSI value.
However, the minimum RSSI value that can received (also called "radio sensitivity") is expected to be smaller with slower communication rates. This information is mentioned in the datasheet of the part.
I hope this will help,
Best regards,