Part Number: CC2340R2
Tool/software:
Hi Team,
We are creating a project for the LE core complete design using QDID 201833, which is listed in SIG by Texas Instruments Incorporated. The QDID 201833 covers the LL and GATT layers, and product owner has not made any changes to these layers. However, during consistency check, we encountered the following errors:
- LL > GAP | If [LL] and [GAP] (8/3) are supported, then [LL] (3/1a) is mandatory.
- LL > GAP | If [LL] and [GAP] (8/4) are supported, then [LL] (3/5a) is mandatory.
- LL > GAP | If [LL] and [GAP] (20/5) are supported, then [LL] (3/4b) is mandatory.
- LL > GAP | If [LL] and [GAP] (20/6) are supported, then [LL] (3/1a) is mandatory.
- LL > GAP | If [LL] and [GAP] (20/7) are supported, then [LL] (3/5a) is mandatory.
According to the PICS selection, LL 3/1a, 3/4b, and 3/5a are mandatory only if LL 3/9 "Extended Advertising" is supported; otherwise, they are excluded. LL 3/9 is not supported by QDID 201833.
We raised a ticket with SIG for assistance in resolving this issue, and we received the following comments:
"If GAP and LL are both in the same QDID, it seems there was an error in the 201833 listing, so this invalid condition is correctly being shown. If you are unable to make changes to the GAP layer, please reach out to your supplier and ask them to submit an ICS Correction Request via a support request."
Regards,
Shammi