Part Number: BOOSTXL-ULPSENSE
Other Parts Discussed in Thread: LP-CC2652R7
Tool/software:
Hi Team,
I have a question regarding the "Analog light sensor for ULPSENSE" SCS example.
Now I am trying to run this example but it gives a warning at the beginning saying:
Board function "BP:Light Snesor / Potmeter" is not connected to an I/O pin on the target chip on this board.
The message suggests a workaround which is to replace the ADC light jumper with a wire to pin 25 and then map the Analog light sensor output to DIOS 27.
I have connected the Light ADC SELECT pin to pin 25 using a jumper wire and mapped output to DIOS 27 as described.

However, I get quite a strange output:

During this graph, I used my mobile flash and then tried to dim the sensor with my hands, but not much can be seen.
Is such signal typical? Can this be a setup issue?
Thank you in advance.
Best regards,
Ahmad