Part Number: CC2340R5-Q1
Other Parts Discussed in Thread: CC2340R5, SYSCONFIG
Tool/software:
I am new to BLE and i am Using CC2340R5 launchpad, and using Basic_BLE project. i want to just broadcast data every 50 sec with incrementing packet number in every advertisement packet. So i changed the sysconfig settings from peripheral to broadcaster. below images are my sysconfig settings.

In order to change broadcasting data i followed Training module steps i made changes in app_broadcaster.c file as shown below
void Broadcaster_AdvEventHandler(uint32 event, BLEAppUtil_msgHdr_t *pMsgData)
{
switch(event)
{
case BLEAPPUTIL_ADV_START_AFTER_ENABLE:
{
MenuModule_printf(APP_MENU_ADV_EVENT, 0, "Adv status: Started - handle: "
MENU_MODULE_COLOR_YELLOW "%d" MENU_MODULE_COLOR_RESET,
((BLEAppUtil_AdvEventData_t *)pMsgData)->pBuf->advHandle);
/** New Code **/
BLEAppUtil_AdvEventData_t * pkt = (BLEAppUtil_AdvEventData_t *)pMsgData;
if (pkt->pBuf->advHandle == broadcasterAdvHandle_1)
{
bStatus_t status = FAILURE;
status = GapAdv_prepareLoadByHandle(broadcasterAdvHandle_1, GAP_ADV_FREE_OPTION_DONT_FREE);
if (status != SUCCESS)
for(;;); // Loop
advData1[0] = 0x02;
advData1[1] = GAP_ADTYPE_FLAGS;
advData1[2] = GAP_ADTYPE_FLAGS_BREDR_NOT_SUPPORTED | GAP_ADTYPE_FLAGS_GENERAL;
advData1[3] = 0x03; // length of this data
advData1[4] = GAP_ADTYPE_MANUFACTURER_SPECIFIC;
advData1[5] = MACaddress[5];
advData1[6] = MACaddress[4];
advData1[7] = MACaddress[3];
advData1[8] = MACaddress[2];
advData1[9] = MACaddress[1];
advData1[10] = MACaddress[0];
if(packet_no<=255)
packet_no++;
else
packet_no=0;
advData1[11] = packet_no.;
broadcasterAdvHandler.eventMask = BLEAPPUTIL_ADV_END_AFTER_DISABLE;
| BLEAPPUTIL_ADV_SET_TERMINATED;
| BLEAPPUTIL_SCAN_REQ_RECEIVED;
status = GapAdv_loadByHandle(broadcasterAdvHandle_1,
GAP_ADV_DATA_TYPE_ADV,
ADV_MAX_LEN,
advData1);
if (status != SUCCESS)
for(;;);
/** End New Code **/
}
break;
}
case BLEAPPUTIL_ADV_END_AFTER_DISABLE:
{
MenuModule_printf(APP_MENU_ADV_EVENT, 0, "Adv status: Ended - handle: "
MENU_MODULE_COLOR_YELLOW "%d" MENU_MODULE_COLOR_RESET,
((BLEAppUtil_AdvEventData_t *)pMsgData)->pBuf->advHandle);
break;
}
default:
{
break;
}
}
}
but the packet no. incremented just once . and when i debugged it, by setting a breakpoint , i found that program counter came into this function only once. how can i change the advertising packet dynamically. kindly help on this