Tool/software:
Hi Team,
We have two CC2340R5 launchpad board, with one acting as a central device and the other as a peripheral. I used the basic BLE SDK without making any changes, only configuring one device as a peripheral and the other as a central. My question is: in connected mode, do BLE devices continuously exchange information to maintain the connection? If so, how many bytes are exchanged, and is there a method to find out?
Board:-LP-EM-CC2340R5
SDK:simplelink_lowpower_f3_sdk_7_40_00_64
Your assistance would be greatly appreciated.
Thanks & Regards
Ratan