This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2340R2: Bluetooth 5.3 without RTOS

Part Number: CC2340R2
Other Parts Discussed in Thread: CC2340R5

Tool/software:

I am working on project that requires sensing 10 sensors (through SPI, I2C and ADC) and sends the data to the mobile application via BLE 5.3 protocol. I thought of using LP-EM-CC2340R5 evaluation board which have 36KB of SRAM. But, upon compilation of the example from Simple Link SDK in RTOS folder called "basic_ble" this example itself occupies 31.3KB (i.e. 85%).

I thought of removing RTOS so that the SRAM consumption will be reduced. But I don't see any BLE examples in nortos folder of Simple Link SDK. My questions are

1)Do you have any examples of BLE transmission without rtos?

        -if no whether BLE 5.3 stack is compatible enough to be developed without using any OS

  • Hello Ruthrapathy,

    Thanks for reaching out. Correct, Bluetooth LE examples require RTOS to work. You can take a look the propRf examples (not Bluetooth LE protocol) inside the SDK: \examples\nortos\LP_EM_CC2340R5\prop_rf.

    BR,

    David.