Other Parts Discussed in Thread: LPSTK-CC1352R, ENERGYTRACE, CC1352R
Tool/software:
Hello! I'm using the LAUNCHXL-CC1352R Launchpad, connected to the LPSTK-CC1352R Sensortag via a JTAG cable.
I'm trying to use EnergyTrace to capture the energy and current consumption of the Sensortag, but no data is appearing in the EnergyTrace chart.
I've removed all the jumpers on the Launchpad and connected the RX/TX pins of the Launchpad to the RX/TX pins of the Sensortag. The Sensortag is powered by 2xAAA batteries.
Could the connection be incorrect? If so, what is the correct wiring setup to use for EnergyTrace to properly capture data from the Sensortag?
Below are the EnergyTrace settings under Advanced Settings, along with a screenshot of the EnergyTrace chart.