Part Number: CC2564CMSP432BTBLESW
Other Parts Discussed in Thread: CC2564C
Tool/software:
HI team,
CCS12.5 IDE with CC2564c MSP432 Bluetopia SDK and imported project and build successfully. getting below commands,
Tried many ways to connect but its only pairing with the mobile unable to connect .
Bluetooth Stack ID: 1
WBS Support initialized.
Device Chipset: 4.1
BTPS Version : 5.1.1.0
Project Type : 6
FW Version : 12.26
App Name : HFP_demo
App Version : 0.5
LOCAL BD_ADDR: 0xC8DF8425682B
GAP_Set_Connectability_Mode(cmConnectable).
GAP_Set_Discoverability_Mode(dmGeneralDiscoverable, 0).
GAP_Set_Pairability_Mode(pmPairableMode).
GAP_Register_Remote_Authentication() Success.
*******************************************************************
* Command Options: Inquiry, DisplayInquiryList, Pair, *
* EndPairing, PINCodeResponse, PassKeyResponse, *
* UserConfirmationResponse, *
* SetDiscoverabilityMode, SetConnectabilityMode, *
* SetPairabilityMode, *
* ChangeSimplePairingParameters, *
* GetLocalAddress, GetLocalName, SetLocalName, *
* GetClassOfDevice, SetClassOfDevice, *
* GetRemoteName, OpenHFServer, CloseHFServer *
* ManageAudio, AnswerCall, HangUpCall, *
* PlaceCallOnHold, HoldingMultipartyCall *
* HoldingMultiPhonesCall, 2PhonesCallAudioSwitch,*
* 2PhonesAnswerCall, QueryActiveConnections, *
* Help *
*******************************************************************
Using the above commands ,please help us to connect and work on it.
Thanks and Regards
Chandra shekar .