Tool/software:
Hi,
We would use ROM serial boot loader to program a blank device. I want to double confirm the following are correct:
1. According to TRM 8.5.2 table, the default BSL_invoke pin is DIO21_A10 (Pin No.13 in RHB package). Is that correct?
2. This default BSL_invoke is “active-low digital input used to start the BSL during boot, need to keep low status when programming”. Is that correct?