Tool/software:
Hi,
In EVM schematic, I assume L1 and C105 are used to fulfill the requirement of datasheet pg.17, “7.4 Note(2) A 10uH and 10uF load capacitor are required on the VDDR voltage rail. They should be placed close to the DCDC output pin.” which is not a problem to us.
The 10uF capacitor placement we want to check is at datasheet p.18, “7.5 Note(1) A 10 µF capacitor is recommended at VDDR pin.” Where should we place this another 10uF at RHB package? VDDR Pin#1 or VDDR Pin#27?