Part Number: DLPNIRNANOEVM
Tool/software:
Hello,
I am currently working with the DLPNIRNANOEVM device over Bluetooth. I can communicate with it using Bluetooth from my PC via Python and the Bleak library.
I want to initiate a scan and store the result of the scan.
When I start a scan, I receive a notification :
bytearray(b'\x01\x83\n\x00\x00')
Similarly, when the scan ends, I receive another notification :
bytearray(b'\xff\x05\x00f\x00')
Could you clarify whether the scan index is 0x01830000 or 0xff050000?
Is it with the command "Request Serialized Scan Data Structure" that I can obtain the scan data?
Once I have the scan data, should I use the DLP Spectrum Library with the dlpspec_scan_interpret() function
Do you have a simple code example?
Thank you for your guidance,
Best regards,
Kilian