This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP-EM-CC2340R5: MCU Boot for OAD On Chip is directly booting the persistent application

Part Number: LP-EM-CC2340R5
Other Parts Discussed in Thread: CC2340R5

Tool/software:

Hi, I am using CC2340R5 and trying to implement On Chip OAD Example. The CCS version being used is 12.8.1 .The flashing process which I am using to flash is as :-

https://software-dl.ti.com/simplelink/esd/simplelink_lowpower_f3_sdk/8.20.00.119/exports/examples/rtos/LP_EM_CC2340R5/ble5stack/basic_ble_oad_onchip/README.html

2. After which I am using my IOS to connect to the device, the device is showing the device name as Persistent App, but as per my understanding mcu boot should load the ble_oad_onchip firmware and as per that in my ios I should be able to see the device name as Basic BLE Project. 

PS:- I used Red and Green LED on the board to verify the above behavior and the results were as expected. The mcuboot is booting the persistent app directly after reset. 

Any clarity on this would be helpful.

  • Hello Sushant,

    Thanks for reaching out. Could you please follow the steps described in this training material: https://dev.ti.com/tirex/explore/node?node=A__AbMoFvWD.bZAg65tD.7NsQ__SIMPLELINK-ACADEMY-CC23XX__gsUPh5j__LATEST
    Also, could you please try directly with the mcuboot hex file from \examples\rtos\LP_EM_CC2340R5\ble5stack\hexfiles for a quick sanity check.

    Best Regards,

    David.

  • Hello David, 
    Thanks for your quick response. I already did followed the training material and I am literally not able to understand why the persistent application is getting loaded by the mcuboot.

    However when I do try to use the mcuboot_on_chip hex file directly it is working fine. 

    But still I want to modify my mcuboot for my application development and I dont know from where can I find the source code for the particular hex file. 

    Please do let me know if something can be done.

  • Hello Sushant,

    I see, thanks for trying that.

    What might be happening here is that the slot size defined for the OAD image is not the same as the one configured in the MCUBoot project. Please make sure the slot size (BOOT_SECONDARY_1_SIZE) in flash_map_backend.h (inside mcuboot project) is the same as the slot size defined in the post build steps of the oad on chip example.

    BR,

    David

  • Hi David,

    I did changed the slot size defined in the post build steps of the oad on chip example, to same as that of the BOOT_SECONDARY_1_SIZE defined in flash_map_backend.h , but still no luck. 

    Below are some screenshots for better understanding.:-

    Please do let me know if something else can be done. Thanks for your constant support.

  • Hello Sushant,

    Please make sure the address you are flashing the application bin file is the same as the address of the secondary slot. I think this is 0x00043000 in your case.

    BR,

    David.

  • Thanks David, for your constant support. The problem is resolved.

    The base address for the oad application and the persistent application has to be updated in the flashmap backend.h in the mcuboot example.

    So the base address of persistent application is 0x00006000, same has to be updated in flashmap backend.h file of the mcuboot example.

    So the base address of oad_on_chip application is 0x00032000, same has to be updated in flashmap backend.h file of the mcuboot example.