Tool/software:
Hi,
I have a couple of layout questions for the CC2651R3SIPA:
First, I am trying to evaluate whether we would be able to use the internal antennae on the CC2651R3SIPA module given a particular board constraint. The board is shaped in a roughly 1.25" circle. Because of this, the 10mm ground plane (G) would get cut off by the edge of the board. See image below for example. The green is the ground plane. Dark Grey is the board. Light Grey is the module. Does this shape violate the recommended design layout? Would this layout put us at risk of voiding the radio certifications?
Second, it is unclear to me how far the 10mm ground plane requirement extends along the module. Does it stop at the 3.2 mm (D) dimension? or does it extend the full length of the module? See image above.
Third, does the 10 mm dimension (G) ground plane need to be clear of components and signal / power traces on all board layers?
Fourth, for the alternate module layout guidelines, the dimension F is listed at 12.98 mm. Is this correct? The dimension G is still listed at 10 mm which means the math does not add up.
Thanks,
Paul