Tool/software:
Hi,
I am currently using the CC2340R5 as a peripheral role for my development. I have used the Basic_BLE code provided in the SDK. The SDK version that I am currently using is "simplelink_lowpower_f3_sdk_8_10_01_02"
I have followed the steps shown in Resource Explorer for enabling passkey entry. Link used is this. One change that I have done here is that I have set the BD address to Public as shown below.
I am able to successfully generate the passkey and bond with a client device. The issue that I have is with the bonding information, The CC2340R5 running the peripheral code is not saving the bonding information after pairing.
Please help me understand how to store the bonding info on the peripheral device.
Thanks,
Sandeep Singh