This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2340R5: One LGPTimer with 2 different frequency PWM output?

Part Number: CC2340R5


Tool/software:

Hi teams,

With the limited hardware resource, I only have one LGPtimer left.

Is it possible to output 2 different frequency PWM by two channels?

PWM1: 1kHz duty 1/5

PWM2: 3kHz duty 1/3

Or is there any other recommended solution ?

Thanks,

BR,

Connor.