Tool/software:
Good Afternoon,
I can't connect well to the persistent app with SimpleLink Connect when I set advertising to 2000 ms instead of 100 ms.
TI SimpleLink Connect: 1.3.7
Chip: CC2340R5
it seems that on Iphone I connect directly without any problem but with another android phone I have problems. I don't know if it is link to the phone or maybe it is coincidence.
My goal is to be able to load an application into the chip with more or less any phone in your pocket
I need to increase the advertising in order to reduce power consumption.
When I use NRFConnect mobile app to connect, there's no problem.
Do you have any idea to fix that ?
Thank you in advance,
Regards
Yohan