This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2340R5: wireless-MCU to manage the control of two 12V DC motors (using the DRV8231ADSGR chip)

Part Number: CC2340R5

Tool/software:

Hi Team,

I need your support on the following request:

#####################################

Is it possible to use the CC2340R52E0RKP wireless-MCU to manage the control of two 12V DC motors (using the DRV8231ADSGR chip) and simultaneously manage the wireless stack using a single Cortex M0 (the chip does not have a core dedicated to the RF section)?

In our application, the two boards must continuously exchange status information and the RX board, at the same time, must move two DC motors, controlling their position using a position sensor.

Regards,

Fabio