Tool/software:
Hi Sir/Madam
I searched in the forum for my issue. Most of the similar problems were solved but mine wasn't.
My btool version V1.44.03 (BLE5)
After programmed with Flash programmer 2 successfully, we can't touch this chipset by using Btool.
Maybe some setup about Btool will be needed
[1] : <Info> - 06:44:31.104
Port opened at 2024/12/23 18:44:31
--------------------------------------------------------------------
[2] : <Tx> - 06:44:31.160
-Type : 0x01 (Command)
-OpCode : 0xFC1D (HCIExt_ResetSystemCmd)
-Data Length : 0x01 (1) byte(s)
Type : 0x00 (0) (Chip Reset)
Dump(Tx):
0000:01 1D FC 01 00 .....
--------------------------------------------------------------------
[3] : <Error> - 06:44:33.176
Message Response Timeout
Name = HCIExt_ResetSystemCmd
OpCode = 0xFC1D
Tx Time = 06:44:31.160
--------------------------------------------------------------------
[4] : <Warning> - 06:44:33.238
Device Reset Timeout
Device May Not Function Properly
--------------------------------------------------------------------