Part Number: CC2340R5
Tool/software:
Good afternoon,
Chip: CC2340R5
SDK:simplelink_lowpower_f3_sdk_8_10_01_02
I want the service Generic Access with 2 characteristic:
-Device Name
-Appearance
and I want to remove the following characteristic (I have to follow a specification that does not allow me to have it):
-Peripheral Preferred Conenction Parameters
-Central Address Resoltion
-Resolvable Private Adress Only

I thought I read in an old post that it wouldn't be possible to remove the service and sub service them because it would be part of the BLE specification.
CC2340R5: Modify Generic Address - Bluetooth forum - Bluetooth®︎ - TI E2E support forums
After reading the BLE specification, I don't see any obligation to keep it.
Which chapter states that they should be mandatory? or how to remove this 3 characteristic ?
Thanks you,
Regards,
Yohan