Part Number: CC2640R2F
Other Parts Discussed in Thread: CC2640
Tool/software:
Hello,
The customer is using CC2640R2FRSMT and has the following two questions. Please help answer them.
Question 1: What are the main functions of the π - shaped network shown in the figure below? What is the function of a 12pF capacitor?

Question 2: As shown in the following figure, how to configure the parameters of "Cap array Trning" in the official CC2640 DTM program? Is there a corresponding table between the values of this array and the specific capacitance values?


Thanks!